Motor_L
Motor_L
| Address: | 8194 (2002H) |
| Type: | DWORD |
| Access: | Read/Write |
| Unit: | µH |
| Range: | DWORD |
| Default Value: | 2420 |
| Store Supported: | Yes |
| Description: | This object sets the motor L (inductance). This value is used when bit #9 of Drive_Working_Settings_Extended object is equal to 0. |
| Notes: |
-- |